The big problem is the microcontroller pins, which often break and make the chip unusable.My idea is to use the terminals of the microcontroller as a plug, on which you can immediately put the socket on and attach the microcontroller with screws. In ...
Future time requires minimizing the cost of chemical elements. In addition, robotics is gaining power. Your chips will improve. It will be necessary to reduce the nodes, microcircuits and their functions. The work of microcontrollers in closed contai...
Hi Team,We are using the L9823 chipset and it is interfaced with imx9qm SOC over spi.Now, I gone through the code of linux kernel but I cann't see any linux kernel driver for L9823 ST chipset.can you please help us to get the linux kernel driver of t...
Page 6 of the datasheet for the M95M04-DR EEPROM has the commands for RDID/RDLS and WRID/LID listed as the same exact commands.Can someone please post the correct command set for this part.
We would like to confirm questions below.ST_M24512-r1. Do you have datasheet for information about SCL speed and minimum Vcc? 2. Is our understand correct that the minimum Vcc of ST_M24512-r is 1.8V with our using SCL 400 khz ? 3. Related no.2. ...
Please check who is Broadcom Account Manager in ST Micro, and please reach me at:sean-sc.chen@broadcom.com
Hi,Can USBLC6-4SC6 be used to protect an IO from EFT (IEC 61000-4-4) and lightning (IEC 61000-4-5)? I do not see any specification for these standards? Thanks.RegardsGordon