HelloI am looking for the BSDL file for the STPC ATLAS PBGA516 processor.X86 Core PC Compatible Information Appliance System-on-Chip.Does anyone have this old filethanks in advance
I'm using M95M02 EEPROM with SPC57 MCU development board. And i've been trying to get a data out from SPI and the data seems corrupted for some reason. I used the same device with an arduino to verify and it works fine so there's no issue withe the ...
Hi,During the holidays, my dad asked me to fix an old device of his. There doesn't seem to be any visible damage (eg. leaking caps or corrosion on the PCB), so I wanted to check if all the ICs on it are still functioning correctly. However, for many ...
I had an idea for debug microcontrollers, so that there were microcontrollers with a light display of the receive-transmit channel. Such chips will be in the category of debug chips, when a circuit is being developed and it is much easier for the cod...
Hi, latelly I am trying to use the buck switching regulator ST1S03PUR and I have some problems with it. It should be something easy to do but seems like not.I have a DC Vin 12V and i want as out 3V3 and 500mA.For the Vout I am using the formula from ...