Other: hardware

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello, I hope i am posting this to the correct area.. I am looking for some help/guidence implementing the VNN1NV04 3-terminal protected MOSFET.

The application is a solenoid driver, 12V 0.5A running PWM 1Khz. It's a very basic low side application, diode across the coil. The signal is 5V logic from a microcontroller.I have read the datasheet, and the application note AN4798. to be honest som...

Spwf04s could not turn on radio afer reset? The module work ok before. Now the radio could turn on after power on . Then initiate and reset wifi module.The radio could not work . why?

[17:13:18.309]ÊÕ¡û¡ô+WIND:1:Poweron:171117-0328fe3-SPWF04S+WIND:13:Copyright (c) 2012-2017 STMicroelectronics, Inc. All rights Reserved:SPWF04SC+WIND:65:Factory Reset:1+WIND:0:Console active+WIND:3:Watchdog Running:20[17:13:19.307]ÊÕ¡û¡ô+WIND:32:WiFi...

Wsl by Associate
  • 374 Views
  • 1 replies
  • 0 kudos