Others: hardware and software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Exactly how much is endurance?

HiWe are using 95128-A125. It's datasheet provides "write cycle endurance" numbers for various operating temperatures. But there is a note that reads "The Write cycle endurance is defined for groups of four data bytes located at addresses [4*N, 4*N+1...

PRana.3 by Associate
  • 602 Views
  • 2 replies
  • 1 kudos

I'm using RH-PMICL1AK1 which is Engineering model of RHRPMICL1AK01V , its datasheet If the voltage drop on RSENSE exceeds 100 mV, the device enters the current limitation mode.However,actually only the voltage drop on RSENSE exceeds 125 mV.

hello,everyone:I'm using RH-PMICL1AK1 which is Engineering model of RHRPMICL1AK01V , its datasheet If the voltage drop on RSENSE exceeds 100 mV, the device enters the current limitation mode.However,actually only the voltage drop on RSENSE exceeds 12...

Dzefa.1 by Associate
  • 649 Views
  • 0 replies
  • 0 kudos

Pin 1 Identification on Part ST L9637D

I have just purchased some samples of the ST L9637D from my local supplier, however Pin 1 Is not identified See attached ImageThe following is printed on the ICL9637DGK924Any suggestions woudl be appreciatedThank you

Steve19 by Associate
  • 829 Views
  • 1 replies
  • 0 kudos