M48T201V Example code
Hello, I recently got a board I designed with the M48T201V and a 4MB SRAM chip. I cannot find any example code for the M48T201V, with or without the memory. Does anyone have any examples? Thank you, Drew
Hello, I recently got a board I designed with the M48T201V and a 4MB SRAM chip. I cannot find any example code for the M48T201V, with or without the memory. Does anyone have any examples? Thank you, Drew
Hello and respect, I downloaded the stv0900 data sheet from the site and it was 5 pages, and unfortunately there was no information about the stv0900 pins in it, is it possible to send me the complete document? I need information about its pins and c...
Hello,I am looking for GaN based half bridges or full bridges evaluation board with gate driver for 250-400V and 3.3kW power rating for Dual active bridge DC-DC converter.Kindly suggest evaluation/ development board for the sameThanks & RegardsAbhish...
Hello,I'm a french student in a 2 years intensive class to prepare engineering school entrance exam and I have to present a scientist project to this exam. I choose to work on transistor conduction and switching loss. My problematic is " To what ext...
Hi i wonder if somebody could share the datasheet on this diode i think its actually a z-diode.Regards HarryKimsRTV
Hello, I have looked many places, including Google and the ST website, and I cannot find this microcontroller anywhere. Markings on this controller are the following:6242MCHHES-02-03M22050431Aif someone can provide any information on this and a datas...
how to import this project: https://github.com/lucysrausch/stm32-turbotronik ?I test importing with (EGit - integration for Eclipse 6.7.0) extension from Eclipse market, but not success (Build icon is not active) same if importing from local director...
Hello,we are using the STM6600CS25DM6F in our Project. We have CSRD tied to a 1uF cap, so 10 seconds long press on PB and SR (PB and SR tied together) for a forced shutdown. We use a 5 sec hold to initiate a shutdown via our controller. Once the cont...
Hello, I am Chintan Mevada. I am an Embedded Hardware Design Trainee. I have Find IC that specification have Battery Management I²C controlled, 1-4-cell, 5-A buck-boost solar battery charger with dual-input selector and MPPT.
i am using electromagnetic sensor which is 24volts. in that i only have the connections for power voltage(positive) and the signal. when i am trying to power it with my stm32f411re nucleo board i can see that the power isn't sufficient. so can i use ...