Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC58xC.h SEMA42_tag structure

Hello, there may be mistake in ST library. In reference manual registers are like that.In the library SEMA4_RSTGT has two different addresses for read and write but those are in the same address.With this when I try to reset gate it goes to one of er...

0693W00000LyDMdQAN.png 0693W00000LyDN2QAN.png 0693W00000LyDOeQAN.png 0693W00000LyDNgQAN.png
kb24 by Senior
  • 671 Views
  • 1 replies
  • 1 kudos

Resolved! Read UART Data on interrupt in SPC5 controller.

how to use UARTto receive data on interrupt instead of using this api (sd_lld_read) as this works in blocking mode in while loop.Micro is SPC560P50L3.Is there is an example to use the Uart Rx on interrupt.As we use this method in Stm32.

VKuma.18 by Associate
  • 1144 Views
  • 2 replies
  • 1 kudos

Resolved! Is there any IDE on Linux for SPC5 MCUs ?

Posted on February 28, 2018 at 08:40My company is working exclusively with Linux, and we have interest in the SPC5 MCUs. But I couldn't find any toolchain for Linux. the SPC5-STUDIO is based on eclipse and claim to be an 'OpenSource Integrated Devel...

Resolved! GNU vs GHS

I am using SPC58EC. When I compile same code with GNU and GHS(Green Hills Software) I see different results.int main(void) {     uint8_t mode;   MC_ME.PCTL[15].R = (uint8_t)18; mode = (uint8_t)MC_ME.MCTL.B.TARGET_MODE;   //SPCSetRunMode /* Clear...

kb24 by Senior
  • 3281 Views
  • 15 replies
  • 0 kudos

Resolved! Core0 stuck in IVOR1

Hello, I am using SPC58EC-Disp board. Core2 is already active and has timer interrupts. I need to set a timer interrupt in Core 0. I am trying use PIT0 and PIT0 configuration is done by Core2 so I think I only need to do PIT0 Channel settings. Two co...

0693W00000LxNyuQAF.png 0693W00000LxNp0QAF.png
kb24 by Senior
  • 715 Views
  • 1 replies
  • 0 kudos