Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC5Studio build failure

Posted on January 19, 2015 at 10:45Hello,I am trying to build a project created using SPC5Studio Wizard. The steps used are File->New->SPC5Studio Wizard. Afte this I selected SPC560D-DIS as the product line. Then selected all the drivers with OSLess...

ssk by Associate II
  • 1301 Views
  • 18 replies
  • 0 kudos

SPC56EL70L5 MCU Basic Initialization

Posted on March 01, 2015 at 00:16Dear All, Thanks for the attention. I'm working with SPC56EL70L5DISP Discovery Board using SPC5 Studio as IDE. I've never had any specific experience with such a kind of MCU indeed i'm having some trobles about how...

luigi by Associate II
  • 494 Views
  • 9 replies
  • 0 kudos

Dual Core Mode option

Posted on February 12, 2015 at 15:43Hello, Currently I am using the SPC56EL which gives the user the possibility to use it in LSM (Lock Step Mode) or DPM (Decoupled Parallel Mode). In Application Configuration ==> SPC56ELxx Platform Component ==> Ru...

Patriks by Senior
  • 193 Views
  • 1 replies
  • 0 kudos

Resolved! SPC560D030 - sleep/power down modes

Posted on February 05, 2015 at 13:43Hello members,1. Has anyone tried implementing sleep/power down modes with SPC560Dxx series MCU? I tried going through reference manual (CD00259063.pdf) but hardly any information is available. Any app note or doc...

ssk by Associate II
  • 885 Views
  • 6 replies
  • 0 kudos

Resolved! How CAN Filter Work on Pictus

Posted on February 17, 2015 at 15:46I am testing CAN filtering Function on SPC560P,But am not clear about how CAN Mask working. Configure as following: Rx ID =0, Rx Individual Mask = 0xFFFFFF8; BCC = 1; From my understanding, then the CAN Node can R...

270284440 by Associate III
  • 293 Views
  • 1 replies
  • 0 kudos

Interrupt vector number

Posted on February 18, 2015 at 14:22Hello Members,I am using SPC560D030 for a product. I have connected PE0 and PB1 to use as wakeup. I want to have system wakeup functionality based on CAN request received (PB1) or when a +5V is applied to a pin PE...

ssk by Associate II
  • 938 Views
  • 9 replies
  • 0 kudos

SPC5Studio 3.4.2 is available !

Posted on February 17, 2015 at 15:28SPC5Studio 3.4.2 is available !Dear Users,The 3.4.2 release is now available on the update site.CORE- Patch Mode Issue : CSE Driver (User files)- Generation issue for JAR Files (CSE Driver and Flash Driver)CHIBIOS...

Resolved! SPC560P40 PICTUS - CTU/NORMAL Trigger for ADC

Posted on February 12, 2015 at 15:09I am currently working on a BLDC control application using SPC560P40 (Pictus) microcontroller and making use of the CTU (Cross-Triggering-Unit) to trigger ADC channels related to BEMF reading in closed loop contro...

benone by Associate
  • 339 Views
  • 1 replies
  • 0 kudos

[Solved]DPSI MOSI problem

Posted on February 10, 2015 at 08:33when I use DSPI , I send two frames 16bits per frame, and I monitor that there is a pulse inter frame on MOSI pin (suppose I send two frames  0x00000000 ), it is very strange , I checked step and step,when I set M...

270284440 by Associate III
  • 204 Views
  • 4 replies
  • 0 kudos