User Activity

Posted on July 18, 2016 at 10:44 Hi, I am currently using the software watchdog of SP56EL configured that the first counter time-out will raise and interrupt and the second counter time-out will reset the device. This works fine, but the contr...
Posted on January 28, 2016 at 07:54Hello, I have a system with an SPC56EL60 with CAN communication at 500kBaud/s. 20 messages are send with cycle time of 200ms. I am using SPC5 Studio and the integrated CAN drivers and configured it to have 16 RX an...
Posted on June 17, 2015 at 07:45Hello, For an upcoming project, I would like to use the SPC56EL54L3 controller. But when I was setting up a SPC5 Studio project, I can´t choose this controller in the platform settings because it is not listed. Is the...
Posted on June 08, 2015 at 16:09Hello, Some time ago I had an issue when activating the ''Preemptable ISR'' option in application configuration for SPC56EL. I posted it in the SPC56 forum. Now my software for SPC560P shows also a strange behavior wh...
Posted on May 13, 2015 at 10:58 Hello, I would like to reload PWM duty cycle every 10 PWM periods using DMA functionality. Therefore I configured FlexPWM subodule 0 and DMA channel An array stores 8 different values for VAL3 register which eq...