Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! UART, I2C, SPI. How to use one of these?

Posted on April 22, 2015 at 11:01Hello,I have this ultrasonic sensor(HY-SRF05 blue): cf in attachment.I have to manage 3 of this sensors simultaneously. How? I have the board SPC560P-DISP. In datasheet there's written of to use the I2C interface or ...

gl2 by Associate III
  • 2996 Views
  • 8 replies
  • 0 kudos

Linking external object files

Posted on October 31, 2016 at 10:05Hello,I have some closed-source library code, which I need to use in my project.If I just add the headers and the .o files to my project, when I build, I get the linker error ''undefined reference to xxx ...''. I n...

SPC5Studio IVOR2/3 Handler

Posted on November 07, 2016 at 06:10Hi,Has anyone used IVOR2/3 Handler using SPC5Studio? I would like to how to write IVOR2/3 Handler routine using SPC5Studio.Thanks and Regards,Dinesh Rode

dinesh by Associate
  • 624 Views
  • 1 replies
  • 0 kudos

SPC5Studio Build and Debug Problems

Posted on October 31, 2016 at 12:57Hello,I'm new to SPC5Studio environment and experiencing some problems using it. I'll be glad if you can help about the following issues:1) When I try to create a project using steps ''File->New->C Project->Makefil...

evren by Associate
  • 730 Views
  • 1 replies
  • 0 kudos

Importing SPC5Studio V3.5 project using V5.0

Posted on October 27, 2016 at 14:46Hi,I need to work on old project created using SPC5Studio V3.5. Project is created using Wizards. When I open same project using V5.0, the 'Configuration.xml' is showing some error (red cross against file name). If...

dinesh by Associate
  • 666 Views
  • 1 replies
  • 0 kudos

Running code from SRAM through BAM loader

Posted on October 17, 2016 at 21:10Hello, Does SPC5Studio provide a way to configure the toolchain to link code to the appropriate address to run from the BAM bootloader, or should I just modify the generated application.ld as I see fit? My goal is ...

SPC5 studio - placing variables at fixed RAM addresses

Posted on September 27, 2016 at 10:54Hello everyone.I�m working on a Bolero microcontroller (SPC560D40L3) using SPC5Studio and Hightec Compiler.I have a question related to variables to be located in RAM.I have a set of global variables, which I nee...

SPC563M64 JATG uncensoring through USB Multilink

Posted on October 13, 2016 at 23:50Hi all. I have some trouble to connect SPC563M64 through USB Multilink. My device is in censored mode with configuration 0xAAAA_AAAA and serial password 0x1122334455667788. I try to uncensor device with this passwo...

cbnsspb by Associate
  • 789 Views
  • 1 replies
  • 0 kudos

PLS UDE and Windows 10

Posted on September 21, 2016 at 11:28Dear All ,in case of Connexion issues with PLS (FTDI Issues) and Discovery Board.Please , install the the last software (4.07.04) coming from PLS websitehttp://www.pls-mc.com/download-spc5-udestk/downloads-a-1626...