Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Questions about SPC5 Studio Install and eco system for SPC58 devices

Dear all,I just ordered the SPC58EC-DISP eval kit and thought it's time to start to setup my first program. I downloaded and installed the SPC5 studio and run immediately into the following problems:When I try to install the GNU CC compiler from the ...

mkrug by Associate III
  • 2374 Views
  • 3 replies
  • 0 kudos

Resolved! Unable to connect to SPC58EC-DISP board through UDE debugger.

I am trying to connect to the SPC58EC-DISP board through PLS UDE Starter kit to program and debug the Serial Test Application example provided with the SPC5 Studio IDE. After opening the debug.wsx in the example project file on PLS UDE, an error appe...

AChie by Associate
  • 1557 Views
  • 1 replies
  • 0 kudos

SPC5 and L9907 current budget recommended?

Hello!I am developing a motor controller driver running on a 48V Li-Ion battery. I want to choose the right regulators. Unfortunately I can not use the MCTK-01 as reference because it is supplied via the mains.What is the current budget I should plan...

CTara by Associate II
  • 654 Views
  • 1 replies
  • 0 kudos

Need help in CAN driver development for spc58xx series

Hello expert, I have just started working on Eiger controller and wanted to develop CAN driver for spc58xx series controller. I do have referrence manual but this device seems to be more complex than others. do you guys have any other technical docum...

vchav.17 by Associate
  • 802 Views
  • 1 replies
  • 0 kudos

Unable to install Flash Driver

Hello, I did a fresh install of SPC5Studio 5.8 and I'm trying to install the Flash Driver from Eclipse Marketplace.But all I get is a:No repository found at http://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio/updates5.I also tried to lo...

SPC58 flash and debugging tool

Hello experts,Can SPC5-FLASH and SPC5-UDE be used on SPC58 series MCUs? For example, can the SPC-UDEDEBG tool quoted here be used for SPC58 boards other than the Discovery kit?https://www.st.com/en/development-tools/spc5-udedebg.html I am looking for...

YC by Associate
  • 1395 Views
  • 1 replies
  • 0 kudos

SPC560B jtag debugging

Hello friendsI am working on a SPC560B50L5 microcontroller and I want to learn debugging it.According to"AN4035 Application note" I can do a single step by loading appropriate values in CPUSCR registers. I do everything that is mentioned in Document....

sdrad by Associate II
  • 694 Views
  • 0 replies
  • 0 kudos