User Activity

Posted on September 13, 2016 at 15:16Good day to everyone,I am writing here in order to have some suggestions on the use of timers. I am writing a spc5 application whee I have a lot of operations and I must do various things at specific moments. For...
Posted on May 03, 2016 at 17:51Good morning to everyone.I am trying to have two mocro (SPCEL60 family) tha exchange some bytes. The micros are connected via UART. I am using the serial driver in cluded in SPC5 Studio.Now I am tryong to use chnWrite ...
Posted on March 07, 2016 at 11:18Good morning to everyone.I am trying to figure out how to toggle periodically a digital output pin with a given frequency. The system clock is configure the internal oscillator, so it should be 16 MHz.I set a timer w...
Posted on March 02, 2016 at 15:57 Good morning to everyone. I am trying to erase a flash memory block. I am try not to use the drivers. As now, I managed to program individual memory cells of the flash memory with storage data, following ...
Posted on February 29, 2016 at 16:12Good morning to everyone,I am trying to understand a possible problem I have with tha AD converter of the SPC56ELxx.I am working on a board where an input current is used to set an input voltage to trhe ADC conver...