Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Regarding Can Communication

Hello All,I used the example application of CAN from SPC5 stdio. As mentioned in the application programs LED's are blinking but i was not able to see the msg in Vector CAN case or in the logic analyser. I need to do any extra modification in any fil...

0690X0000089r2yQAA.png 0690X0000089r2UQAQ.png
RRama.8 by Associate II
  • 916 Views
  • 1 replies
  • 0 kudos

SPC5Studio Diadem officially released

Dear All ,SPC5Studio updated components are available (56,57 on 58)more information on http://download.spc5studio.com/you can download SPC5Studio tool in this link :https://www.st.com/en/development-tools/spc5-studio.htmlSPC58xHxx credentials should ...

Resolved! SPC5-CRYP-LIB for SPC560B54

Hi there,I've downloaded the SPC5-CRYP-LIB from the ST website. It says that it should be supported for the whole SPC5xx family, with hardware support only enabled for the SPC560B/C MCU. I am trying to import this plugin for the SPC560B54, but SPCStu...

JVan.1 by Associate
  • 1996 Views
  • 3 replies
  • 0 kudos

download.spc5studio.com

Dear All ,SPC5Studio updated components are available (56,57 on 58)more information on http://download.spc5studio.com/SPC58xHxx credentials should be requested on credentials@spc5studio.comNew or updated componentsCore 1.5.0   Pinmap wizard multiple ...

Resolved! How to handle interrupts in SPC5Studio generated application : boot.s in SPC56EL60L3 (HW/SW mode) ?

 * Unhandled exceptions handler for core 0.     */    .align   2    .weak    _IVOR0, _IVOR1, _IVOR2, _IVOR3    .weak    _IVOR4, _IVOR5, _IVOR6, _IVOR7    .weak    _IVOR8, _IVOR9, _IVOR10, _IVOR11    .weak    _IVOR12, _IVOR13, _IVOR14, _IVOR15    .wea...

Resolved! eclipse marktplace and check for updated Connection failed.

​After Installation of spc5 Studio, i want to download the toolchains. but there is always a Connection error. see below pls: org.eclipse.equinox.p2.transport.ecfWarningWed Mar 13 12:51:45 CET 2019Connection to http://vps182808.ovh.net:8080/marketpla...

bgong by Associate
  • 1678 Views
  • 2 replies
  • 0 kudos