...A14
SWDCLK
Now running STM32CubeProgrammer with this setup, I'm getting "Error: ST-LINKerror (DEV_UNKNOWN_MCU_TARGET)" when using JTAG port and "Error: No STM32 target found......
...After clicking on "ok" reconnect your card with STLINK, then check the device authentication ID by clicking on "Read."
3. Disable the RDP regression with a password.
&n...
...ort 1 If you are trying to connet to a device with TrustZone enabled please try to connect with HotPlug mode Error: DEV_UNKNOWN_MCU_TARGETError: Cannot identify the device Some additional i...
...Error: ST-LINKerror (DEV_UNKNOWN_MCU_TARGET)
2nd connect tentative with a lower frequency (8MHz)
ST-LINK SN : 003D00253038511834333935
ST-LINK FW : V3J6M2B4S1
Voltage : 3.31V
Error: ST-LINKerror...
...in 4, T_JTMS
Pin 6, T_JCLK
Pin 8, T_JTDO
Pin 10, T_JTDI
The connection fails using the CubeProgrammer.
I get the following message: "ST-LINKerror (DEV_UNKNOWN_MCU_TARGET)".
On t...