STM32CubeProgrammer (MPUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeProgrammer 2.15.0 released

STM32CubeProgrammer v2.15.0 release informationNew features:• Added the NOR flash memory and OTP fuse programming via USB and UART using OpenBootloader for the STM32MP13xx microprocessors• Added the support for the PMIC programming via UART for the S...

STM32CubeProgrammer 2.15.0 released

STM32CubeProgrammer v2.15.0 release informationNew features:• Added the NOR flash memory and OTP fuse programming via USB and UART using OpenBootloader for the STM32MP13xx microprocessors• Added the support for the PMIC programming via UART for the S...

Error installing stm32cubeproj 2.12.0 SEVERE: com.izforge.izpack.api.exception.IzPackException: Console implementation not found for panel: com.st.CustomPanels.AnalyticsPanels

WORKING:> sudo java -jar SetupSTM32CubeProgrammer-2.11.0.exeFAILS> sudo java -jar SetupSTM32CubeProgrammer-2.12.0.exeCompletely uninstalled JAVA, then reinstalled - no change.Reviewed several community posts, no solution yet.Environment: macOS Big Su...

GJet7 by Associate
  • 703 Views
  • 5 replies
  • 3 kudos

STM32CubeProgrammer 2.14.0 released

STM32CubeProgrammer v2.14.0 release information New features:• Updated the support for the entire STM32H5 series: – Debug authentication with password or certificate – Authentication key provisioning – Key generation – Firmware encryption and signing...

Select boot mode for M4 examples not showing

Hello,The starter package of STM32MP1-Ecosystem-v4.1.0 is downloaded to the SD card on STM32MP157D-EV1 board and SD booting is fine as attached log file. The tried layout files were FlashLayout_sdcard_stm32mp157d-ev1-trusted.tsv and FlashLayout_sdcar...

JKim.2 by Associate II
  • 301 Views
  • 0 replies
  • 0 kudos

Resolved! Reading and writing RAM via ST-Link

I am using STM32MP153 MPU on custom board.Is it possible to read/write memory region using ST-Link connected via JTAG interface?Most interesting if this is possible through some command line interface, perhaps my own C program using some API.

axel101 by Associate III
  • 963 Views
  • 6 replies
  • 0 kudos