STM32 MPUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Remoteproc error

Hello,I have compiled a custom image to run on the M4 core on my stm32mp157f-dk2. I generated the code using STM32CubeMX. I am able to build it fine but am having issues launching it on the m4 core. Here are the commands that I run. echo executable.e...

Resolved! question about stm32mp1 LTDC PIN configuration

Hi,My LCD display format is RGB666, I removed the "LCD_R0,LCDR1, LCD_G0,LCD_G1,LCD_B0,LCD_B1" in file "stm32mp15-pinctrl.dtsi", and recompile my device tree, then upload to my board. I tried to use the LCD_R0 as GPIO with command: gpioset gpiochip7 2...

zqizh.1 by Associate II
  • 664 Views
  • 3 replies
  • 0 kudos