2022-02-13 7:55 AM
After buildroot I'm trying to get the yocto build to work. I'm using openstlinux-5.10-dunfell-mp1-21-11-17. The boot process always stops on SP_MIN: Preparing exit to normal world. Yes, I have already read the https://st.force.com/community/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide. I do have the memory correct and I do not have any pins configured in &rcc. The same device tree file(s) works on buildroot. How can I debug this? The board I'm using is from MYiR (MYD-YA157C).
Edit: I'm using custom machine, which is defined in layers/meta-st/meta-st-stm32mp-addons/conf/machine
2022-02-25 11:56 AM
I’m not really getting any further. Anyone any suggestions how to proceed? @OlivierK Can you help here?
2023-02-07 10:37 AM
Try reading and adapting this patch file. It is needed when you remove CONFIG_ENV_IS_NOWHERE=y from the u-boot defconfig
2024-08-09 5:38 PM
Hello, have you resolved the issue?
Thanks, Dominik.
2024-09-05 6:07 AM
Try to enable debug messages in CONFIG/menuconfig to get more clues
Symbol: DEBUG_LL
Depends on: DEBUG_KERNEL
Location:
-> Kernel hacking
-> arm Debugging
[*] Kernel low-level debugging functions
Symbol: STM32MP1_DEBUG_UART
Location:
-> Kernel hacking
-> arm Debugging
[*] Kernel low-level debugging functions
[*] Kernel low-level debugging port
(X) Use STM32MP1 UART for low-level debug
Symbol: EARLY_PRINTK
Depends on: DEBUG_LL
Location:
-> Kernel hacking
-> arm Debugging
[*] Kernel low-level debugging functions
[*] Early printk
Change extlinux.conf (found on the bootfs) to include earlyprintk
root=/dev/mmcblk0p6 rootwait rw earlyprintk console=ttySTM0,115200`