User Activity

Hello, I am having an issue when I try to download the Developer package in the wiki. I am using this link (https://wiki.st.com/stm32mpu/wiki/STM32MPU_Developer_Package#Installing_the_Starter_Package) in the 5.2 section, there, it redirects me to (ht...
Hello, I am developing a custom image using the layer meta-st-stm32mp in the mickledore branch, until that point, there are no problems.The problem is, since I want ti install the meta-st-x-linux-ai layer, I need to install meta-st-openstlinux first,...
Hello,I am trying to configure a PWM in the boot process. I followed the steps in the documentation https://wiki.st.com/stm32mpu/wiki/TIM_device_tree_configuration .I configured the pwmleds nodepwmleds { compatible = "pwm-leds"; example { labe...
Hello, I hope you are doing well. I have developed a custom PCB with the STM32MP153AAB microprocessor. The process followed  almost all the steps in the wiki for the STM32MP157F-DK2 discovery kit, however, some pins had to change due to the custom de...
Hello, I'm trying to develop a SOM device with a STM32MP153AAB3 processor, I would like to use the 2BC CYW4373 chipset, since it's dual band wifi  module. The reason why  I want to use this chip is because I want to be able to use it as an Access poi...