STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
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
Gfang.2
Associate II
since
2023-03-22
2023-06-14
User statistics
10
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About Gfang.2
Options
Report User
User Activity
Posts
Replies
How to import X-CUBE-NFC5 into the STM Cube IDE project? Which part is imported?
2023-06-05
Editing ST25R3911B DISCO in STM32CubeIDE
2023-05-29
Editing ST25R3911B DISCO in STM32CubeIDE did not generate an error, but it cannot be read. How can ST25R3911B edit NFC in STM32Cube?
How to Add NFC Modules to STM32Cube IDE Software
2023-05-26
ST25R3911B-DISCO use HAL library
2023-05-23
ST25R3911B-DISCO is not suitable for its GUI. Use the HAL library to write programs to read ST25. Is there a related program?
Re: Editing ST25R3911B DISCO in STM32CubeIDE
2023-06-07
Can STM32Cube add X-CUBE-NFC5? If possible, how can I add X-CUBE-NFC5?
Re: Editing ST25R3911B DISCO in STM32CubeIDE
2023-06-05
I am currently using X-NUCLEO-NFC05A1. Can I use X-CUBE-NFC7 to configure ST25?
Re: How to import X-CUBE-NFC5 into the STM Cube IDE project? Which part is imported?
2023-06-05
Thank you, but I didn't find X-CUBE-NFC5 in it.
Re: Editing ST25R3911B DISCO in STM32CubeIDE
2023-05-29
Can the X-NUCLEO-NFC05A1 board serve as a reader for reading data?
Re: How to Add NFC Modules to STM32Cube IDE Software
2023-05-29
I am using the ST25R3911B-DISCO board, which is an NFC reader. Which NFC firmware package does this board use?
View more