cancel
Showing results for 
Search instead for 
Did you mean: 

[IMU] Talking to sensors on sensor hub

BA_
Associate II

So i have a LSM6DSOX and connected to its sensor hub LIS3MDL.

Currently I'm trying to log data to feed into the NanoEdge studio.  So i need to grab data from the actual LIS3MDL.

On the sensor hub you can read and write registers through the sensor hub correct?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @BA_ ,

On github you can find some official examples on how to implement sensor hub using LSM6DSOX and LIS2MDL. You can use them as starting point.

Hope this helps :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
BA_
Associate II

So you set the address to be a read or write SLV0_ADD (15h)

Then with SLV0_SUBADD (16h) you can set the register

Then this is used to write the value DATAWRITE_SLV0 (21h)

But i don't know how a data read works.  Also not sure how you read more then one sensor?

 

 

BA_
Associate II

The read somehow comes from the SENSOR_HUB_1-18

Federica Bossi
ST Employee

Hi @BA_ ,

On github you can find some official examples on how to implement sensor hub using LSM6DSOX and LIS2MDL. You can use them as starting point.

Hope this helps :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.