Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Question about X-CUBE-AI

I have trained a neural network model and trying to implement it using STM32L476RG Nucleo board. I have generated an application template and the input to the neural network is 32 X 32 X 1. I'm trying to understand below parameters in network_audio_a...

Khoo.B by Associate III
  • 1774 Views
  • 4 replies
  • 0 kudos

I am using STEVAL -STLKT01V1 BOARD . As per schematic the board is conencted to the pin PD2 and PC12 for UART Rx and UART Tx as per Cube MX suggestion , but in the schematics it shows USART Rx and USART Tx. Kindly confirm which is ok.

I am using Keras model to validate the code . I am enclosing the schematic details for your reference.How should I Configure the platform settings of AIwhat should I select here If I select manual following error shows If I select the below setting e...

STMicroelectronics.X-CUBE-AI.6.0.0, Verify the Platform Settings Tab

Hi,i was trying to update my cubeAI pack but cubeide can't unzip this new version.If I use my old projects and I try to change something in the .ioc file a message appeare on my pc:these IPs still have some not configured or wrong parameter values: [...

GLong.2 by Associate
  • 522 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L1 and STM32L0 for running Neural Networks

Can STM32L1 and STM32L0 be used for AI development (is. running inference of neural networks)? I was hoping to use those chips with X-CUBE-AI. Yet, when I read the user manual, those chips were left out of the list of microcontrollers. Why is this so...

Resolved! Device Configuration Tool Console doesn't open in STM32CubeIDE

Hello,Device Configuration Tool Console doesn't open in STM32CubeIDE.I clicked "Open Console -> 4 Device Configuration Tool Console". But the console was not opened.It is important to Validation of X-CUBE-AI application.Thank you.

Yuk117 by Associate III
  • 4572 Views
  • 5 replies
  • 1 kudos