Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST is Looking for Data Scientists – Join a paid usability session

Hello Community,   ST is Looking for Data Scientists – Join a paid usability session   Are you a data scientist or ML engineer with experience deploying neural networks on edge or embedded devices? The ST team is organizing 45-minute remote usability...

Resolved! MLC functionality on MKSBOX1v1

I have this board with STM32L4R9 and I used CubeMX and Unico-GUI tools to generate a decision tree for MLC in .ucf format. I used a python script to convert this to C uint8_t array as follows:   const uint8_t lsm6dsox_ucf[] = { 0x10, 0x00, 0x11, 0x0...

STM Model Zoo Audio Event Detection

I want to train one of the pretrained AI models (lets say i choose yamnet), on my own data. I want to use mimii dataset which consists of different industrial equipment sound files in .wav format in normal working condition and anomalous working cond...

jzzunn by Associate II
  • 623 Views
  • 1 replies
  • 0 kudos

STM32 Model Zoo Help

I have followed the model zoo github tutorial to train, quantize and deploy an Audio Event Detection model. I used the available yamnet-256 and followed the tutorial to the end of deployment. I manage to get successful deployment but when I connect t...

jzzunn by Associate II
  • 712 Views
  • 5 replies
  • 1 kudos

X-CUBE-AI 9.0.0: TOOL ERROR: Error in computation of shapes

Hello, ST community members, I am trying to port an onnx model to STM32H743VITx through X-CUBE-AI. When analyzing the network, the following error message appears:"TOOL ERROR: Error in computation of shapes"I don't know if it is because some layers i...

lc_guo by Associate
  • 1110 Views
  • 3 replies
  • 0 kudos

Resolved! Automatic Validation on target compilation problem

Hello. I have made with ST Edge AI Developer Cloud a model and downloaded the whole project for STM32CubeIDE. When I do Validate on desktop it works fine and I get expected results.But Validate on target gives me a compilation error.  Building projec...

DenDanne_0-1730889104446.png
DenDanne by Associate II
  • 2765 Views
  • 10 replies
  • 3 kudos

.ucf file and LSM6DSO16IS

I have a LSM6DSO16IS (sensor with ISPU) and I want to upload in it its configuration file (.ucf). I only saw guides which shows how to upload it through MEMS Studio or Unicleo GUI, but I want to upload the .ucf without external tools (like MEMS Studi...

lsm6dsv16x temperature sensor and learning tools for mlc and fsm

Hi everyone,I’m evaluating the LSM6DSV16X for a project and have a couple of questions:1. Temperature Sensor AccuracyI know the built-in temperature sensor is mainly for internal monitoring, but I’m wondering how reliable it is for actual ambient tem...

ACand.3 by Associate III
  • 717 Views
  • 1 replies
  • 0 kudos

STM32N6 Image Classification Example code to run on Keil

Hi,     I am using STM32N6570-DK kit. I have an example project for image classification, but it is designed for STM32CubeIDE. I want to port this project to Keil ( in order to use the ARM Compiler). Could you please provide the project file so it ca...

VasuV by Associate II
  • 752 Views
  • 2 replies
  • 0 kudos