STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FWU Metadata partition protection

Hi,I'm looking at the wic file for STM32MP13 and see two metadata partitions for ATF firmware update. I'm wondering how are these partitions secured from access / modifications from non-trusted world? Since write (and optionally read) operation shoul...

pp2 by Associate II
  • 825 Views
  • 3 replies
  • 0 kudos

Resolved! Trouble Flashing STM32DDRFW-UTIL over USB

Background:I'm trying to bring up a custom board with an STM32MP157D and DDR3. When I tried flashing the BSP, I got an error: "ERROR: DDR addr bus test: can't access memory @ 0xc0000004". I decided to try using STM32DDRFW-UTIL to test the DDR before ...

ALeba.1 by Associate II
  • 804 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP153 Custom DTS: TZC Permission Failure

I'm getting the following log when trying to boot to a custom DTS. I've already attempted the suggestion mentioned in this st forum post (https://community.st.com/t5/stm32-mpus-products/op-tee-error-tzc-permission-failure-on-new-v5-0-0-sdk/td-p/58433...

Louis1 by Associate II
  • 844 Views
  • 1 replies
  • 1 kudos

Resolved! How to enable PWM pin

i am facing the issue like i could  not able to access the PWM pinsi want like this only (/sys/class/pwm/pwmchipX/).but i get output like this only. {root@stm32mp1:~# cd /sys/class/pwm/root@stm32mp1:/sys/class/pwm# lsroot@stm32mp1:/sys/class/pwm# ls}...

Resolved! Specific U-BOOT on STM32MP157-D

Hello,I am currently using the STM32MP157D to develop some tests. It seems that a specific U-BOOT has been developed by ST and flashed in the default factory eMMC.On this specific U-BOOT, some self-test commands are interesting.Could it be possible t...

MJ_TS by Associate
  • 805 Views
  • 1 replies
  • 0 kudos

STM32MP13 board not booting into FSBL

Hi, I have a board that I designed that's not booting and I am struggling to workout why.I don't see any output on UART4 when booting and I also noticed that openocd reports the program counter as the following which I believe means that its still in...

joe-bm1 by Associate
  • 796 Views
  • 2 replies
  • 0 kudos

How do I boot from Flash in a Baremetal?

I am using the STM32MP131 in a baremetal environment. Since there is no internal flash, I am planning to use external flash and DDR.I have confirmed that writing to and reading from the flash works, but I don't know how to start from FLASH instead of...

Stnoobs by Associate II
  • 957 Views
  • 4 replies
  • 0 kudos