STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Very slow Ethernet connection on ETH1

We have some devices based on STM32MP257 SoCs that connect to a 100 Mbit Ethernet network via ETH1, where ETH1 is going straight to an RMII PHY. Pins for ETH2 are reserved, but are not used/not connected. Some of our devices work rock-solid as except...

rtie by Associate II
  • 951 Views
  • 9 replies
  • 0 kudos

Resolved! PMIC-related issues

The STM32MP135 is powered by PMIC1A. After initial power-up, the voltage at BUCK4 is normal at 3.3V, but during U-Boot flashing, the output voltage at VOUT4 drops to only 2.4V, causing the flashing to fail. The VDD and VDDQ pins of the eMMC are power...

LH1 by Associate II
  • 307 Views
  • 1 replies
  • 0 kudos

MIPI DSI IBIS MODEL for STM32MP255

Hi, I tried exporting the IBIS model from ST website. On importing model to SI tool I can see that there is no model assigned to DSI lines. It is showing NC. Can you share the IBIS model with MIPI drivers in it. or share some IBIS model which I can u...

DJ_IND_0-1758102381709.png
DJ_IND by Associate III
  • 887 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.