User Activity

According to the wiki here: ROM_code_overview, the pins to boot from a serial NOR flash chip can be modified by the OTP Register. I understand that I must set the bit 0 of the word 3 to 1, but how do I define which function I move to another pin? whi...
Hello, I'm designing a board based on the STM32H735IGK3 microcontroller in which I want to include two HyperBus / OctoSPI memories in multiplexed mode. For this kind of memories there is more avaiblity on 1.8V power supply, but reading the documentat...
Kudos given to