2025-04-23 12:23 PM
Hi STM-Team,
We have the custom board based on the STM32MP157DAC board with KLD35176BVIB LCD display.
KLD35176BVIB is actually BOE3.49(VGA) + HX8394f display.
We are using yocto build to configure the display panel changes.
I have attached my device tree configuration
1) I need to configure below pins.
| Pin Name | Pin Number | Function | Implementation | Remarks |
| PA14 | T2 | TP_INT | Touch Panel interrupt | Reference design has only DSI_LCD_INT, combined for Display + TP |
| PD13 | AA19 | DSI_TE | Pin re-mapped | FUNCTION MOVED FROM PC6 TO PD13 |
| PD15 | J2 | DSI_LCD_BL_CTRL | Pin re-mapped | Function moved from PA15 |
| PH6 | Y11 | TP_RESET |
I was not able to find how and where to map these pins for my display panel As I am not much familiar with ST pin-mapping I was not able to figure out these mappings.
2) I was also looking for the DSI defaul data and clk pins pinmapping in device tree but not able to find it for below pins.
| DSI_D0P |
| DSI_D0N |
| DSI_D1P |
| DSI_D1N |
| DSI_CK_P |
| DSI_CK_N |
| DSI_RESET |
| DSI_LCD_INT |
3) Additionally is there a display driver available for KLD35176BVIB if yes how to enable it an use it to bring up our display LCD if no which alternative driver can we use since i can't find BOE+hx8394f driver in driver/gpu/drm/panel/ files.
4) I wanted to also know what is the best way to make and track device tree changes for linux-kernel,u-boot, and TFA. Since directly making changes in /tmp folder doesn't seem to be the best solution.
Thanks.
Solved! Go to Solution.
2025-06-22 12:18 AM - edited 2025-06-22 12:19 AM
Hello,
I have not configured the TE pin.
The backlight pin is configured using PWM.
The INT and RESET pins are configured and included in the touch panel configuration, which communicates over I2C.
2.
As far as I understand, these pins do not require explicit configuration because they are by default assigned for DSI display communication.
3.
I was able to get the display working by using the HX8394F driver from the Linux Git repository and adding the display initialization sequence provided by the display vendor.
4.
I used the devtool modify command to set up a workspace and track changes using Git commits.
Thank you.
2025-06-22 12:18 AM - edited 2025-06-22 12:19 AM
Hello,
I have not configured the TE pin.
The backlight pin is configured using PWM.
The INT and RESET pins are configured and included in the touch panel configuration, which communicates over I2C.
2.
As far as I understand, these pins do not require explicit configuration because they are by default assigned for DSI display communication.
3.
I was able to get the display working by using the HX8394F driver from the Linux Git repository and adding the display initialization sequence provided by the display vendor.
4.
I used the devtool modify command to set up a workspace and track changes using Git commits.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.