User Activity

HelloWe are Working on STM32MP257F-DK Board.We would greatly appreciate your help if you could help us with the following doubts:We Would like to How to disable ON-Board ST-link and Set it to J-LINK ModeWe want to Check  Ethernet using build root in ...
Hello We have a few queries regarding the use of ST-Link for debugging, and I would greatly appreciate your assistance in this matter.We are currently using a J-Link Base probe for debugging the STM32MP157F processor in SEGGER EMBEDDED STUDIO, and we...
HelloWe have a few questions regarding LPDDR4 memory configurations, and we would appreciate your inputs:What is the maximum capacity of an LPDDR4 memory module with a dual-channel, single-rank (1-Die) configuration, where each channel is 16 bits?Doe...
​Hello We are Working on a custom board with STM32MP157AAA3 processor.We are using Buildroot(V2023.08.2) for checking USB 2nd Port in which the PHY port 2 is configured as host controller using UTMI . we referred the below link to configure the dts :...