STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP15 SWD Issues

Hi,I recently just finished the Yocto Bringup of a custom STM32MP15FAA1. Everything seems to be working in my application. I am now looking to begin development of the M4 in which I need access to either SWD or JTAG to do lower-level development. Unf...

STM32MP153 DRAM Hardware Question

Hi,I'm designing a board with STM32MP153FAD and have a question about DDR layout reference.Which reference should I follow for the DRAM section?Eval kit MB1272C_03 layoutST's published reference DDR layout.Questions:Which is the recommended reference...

foc by Associate II
  • 280 Views
  • 2 replies
  • 0 kudos

Resolved! eMMC and DTS

Dear all,We have a design where the VCCQ of eMMC is currently 3.3V. We need to move to 1.8V to be able to use a new referenceIs there any risk to break somthing if I use the below DTS on board where eMMC is 3.3V VCCQ. We have pull up to VCCQ on D0 an...