STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

dynamic memory size

In the stm32mp157C-DK2 board, there is a DDR3 memory with size 4GB x 1.I wanted to know why the size defined in the system is 512mb as the next figure show :

0693W000003PP7YQAW.png 0693W000003PP7iQAG.png
med by Associate II
  • 880 Views
  • 4 replies
  • 0 kudos

Resolved! Error in recipe st-image-resize-initrd while building openstlinux-5.4-dunfell-mp1-20-06-24

Hello,​I always get following error while building openstlinux-5.4-dunfell-mp1-20-06-24:ERROR: st-image-resize-initrd-1.0-r0 do_rootfs: The postinstall intercept hook 'update_desktop_database' failed, details in /mnt/data/dist-pack/openstlinux-5.4-du...

DmnSd by Associate III
  • 2294 Views
  • 8 replies
  • 0 kudos

Resolved! How to use touchGFX on STM32MP1 ?

Hi @martin KJELDSEN​ , I have some questions related to porting touchGFX on STM32MP1 which are as below : 1) Is it possible to run touchGFX on M4 core available on STM32MP1 ? 2) As I understood earlier touchGFX was supported on ARM processors, If I h...

Shree by Associate II
  • 2164 Views
  • 5 replies
  • 0 kudos

video codec

I am developing an industrial tablet with only one task - to display and record videoIt should be ready to work in a few seconds after turning on (that's why I also think about using STM32H7)I need to show on the display 720p (ideally 1080p) 30 frame...

ltdc-simple panel- parallel DRM mode fail

Hi i have a ltdc tft display RGB parallel display connected to stm32mp15 series,unable t0 get drm link to DPI connector, the code flow is breaking at following files,using DISTRO              = "openstlinux-weston"i have no idea where to start to deb...

Ara.1 by Senior
  • 1071 Views
  • 1 replies
  • 0 kudos

Failed to download system image

Our self-made board contains emmc and lpddr3 (1GB, 32bit). The error message when downloading the image is as the attachment. Use Uart to monitor during the download process to get the following information:NOTICE: CPU: STM32MP157AAC Rev.Z NOTICE: Mo...

YWu.2 by Associate II
  • 2314 Views
  • 8 replies
  • 0 kudos