User Activity

after click on "stm32wrapper4dbg" link, "Permission error" is appeared (authorization doesn't help)
smt32mp157a-dk1/c-ev1 boards. When BOOTSCHEME_LABELS (stm32mp1-eval.conf) is changed from "trusted" to "basic" the build of u-boot-stm32mp recipe fails. Ecosystem 1.2.0 .
Why after$ source ./layers/meta-st/scripts/envsetup.shaliases is empty? What for?
On most cases the script "create_sdcard_from_flashlayout.sh" futile. Built-in card reader today is preliminary remains on notebooks. As result very often a sd-card used over a usb adapter. On a remote virtual machines always it will be used over a c...
During build with DISTRO=openstlinux-x11 IMAGE=st-example-image-x11 MACHINE=stm32mp1-disco on Ecosystem-1.2 errors arose:------------------------------------------------------->ERROR: st-image-vendorfs-1.0-r0 do_rootfs: The postinstall intercept hook...