Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
I enter STM32_Programmer_CLI -c port=/dev/bus/usb/010/003 (lsusb reports this is correct) -w flashlayout_st-image-weston/trusted/Flashlayout_sdcard_stm32mp157c-dk2-trusted.tsvudev drivers installed, Ubuntu 20.04Warning: Wrong connect parameter:
I want to use stm32mp1 chip to drive ssd22288 rgb-mipi screen. Could you give me some solutions?
Sorry if I have come to the wrong group. I am searching for information on why a font would work with some code that already exists and what if the best way to visualise this. Tried a number of softwares and sites but none provide the array that I'm ...
Only the power supply via USB C CN6 allows booting with detection of the presence of voltage on GPIO PA5 and PA4. Is there a way to modify this control mode and be able to boot with a CN2 power supply? Is it possible to modify the FW so as not to re...
I am evaluate the STM32MP157C-DV2 board.I have disabled the weston service by referring to the link below.https://community.st.com/s/question/0D53W00000cSKmXSAW/disable-weston-autostart-in-stm32mp157cdv2When boot with the weston service disabledThe ...
�?러메시지 입니다.Can not connect to target!Please select "Connect Under Reset" mode from Target->Settings menu and try again.If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu....
Hi,AN5122 in paragraph 3.2 recommends to use 33 ohm serial resistor for every A/C of the DDR chip, but the STM32MP1_SeriesDDRmemory_routing_guidelines_examples.zip in STM32MP15XXAA_1DDR3Lx16 example there are NO serial resistor. Can I use this layout...
I am using STM32CubeIDE in Ubuntu20.04.If you create the STM32MP1 project in STM32CubeIDE for Ubuntu, it asks if you want to install the OpenSTLinux SDK. And I have installed it and am using it.However, in STM32CubeIDE for Windows, if you ask if you ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.