Forum Posts
step to integrate the driver to stm32MP157-DK2 with LAN9512
Hii,I am using stm32MP157C-DK2 with the default kernel.I am trying to integrate LAN9512 with stm32MP157C-DK2 I need a step to integrate the driver to stm32MP157-DK2 with LAN9512
How to set up a touchscreen with USB port ?
I'm having trouble setting up a hdmi monitor with a usb touchscreen on the stm32mp157. In the command lsusb it appears, but I can't link it with X11. What is the correct process for configuring the USB touchscreen on this board? I managed to make it ...
Resolved! PLL Calculation on STM32MP157A does not make sense.
I am working on the STM32MP157A. Setting PLL in the STM32CubeIDE does not work as expected. 24 MHz HSE DIVM4 = /5 DIVN4 = X84 DIVQ4 = /5 should = 80,460,000 . The MX program says 80,960,039. I do not understand. If the MX program is right, then what ...
STM32MP157-DK- SUPPORT ON DMA DRIVERS
Hi Team,Please help on DMA driver part of STM32MP157 DK eval board and also the base address for DMA .RegardsSS
Resolved! Questions about setting the spi clock (devicetree file, M4 Core side)
Hi ST.I set the clock in the dts file as below.&rcc { st,hsi-cal; st,csi-cal; st,cal-sec = <60>; st,clksrc = < CLK_MPU_PLL1P CLK_AXI_PLL2P CLK_MCU_PLL3P CLK_PLL12_HSE CLK_PLL3_HSE CLK_PLL4_HSE CLK_RTC_LSE CLK_MCO1_DISABLED CLK_MCO2_DISABLED >; st,clk...
[WEBINAR] Accelerate your STM32MP1 MPU design with SiP and SoM solutions
Join our 1-hour webinar to learn how System-in-Packages (SiPs) and System-on-Modules (SoMs) can optimize your MPU-based design and boost time to market!Register Now !
Create a 32b parallel bus
Hello, I am working on the stm32mp157-dk1. I would like to create a 32bits parallel bus on cortex A7, at a frequency greater than 20Mhz but when I do a test on a pin I get a max frequency of 120khz, which is too low. I think this is the wrong program...
Understanding the functions of Remoteproc
Hi,iam a bit confused aboute the remoteproc framework and if my understanding of it is correct.In my view, the remoteproc framework can start the m3 firmware with having its elf-file in a dedicated place of the filesystem. The remoteproc also parses ...
STM32MP157A-DK1 UART3 kernel module
Hy wanted to make a kernel Module and i wanted to know whats the best way to acces the uart from Kernel Space.So far i enabled the UART in the device try and now i am able to send data. But now i know since the uart us in userspace i cant access it f...