STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi,i am a beginner in MPU development. I have created cortex-M4 firmware project using stm32cubeide , but how can i start my firmware at the time of bootup?

i have read the article, https://wiki.st.com/stm32mpu/wiki/How_to_start_the_coprocessor_from_the_bootloader#Starting_the_coprocessor_firmwarewhere will i find this in my device tree#define CONFIG_EXTRA_ENV_SETTINGS \ "stdin=serial\0" \ "stdout=serial...

AGupt.8 by Associate II
  • 10868 Views
  • 13 replies
  • 0 kudos

i2s1 mclk genration patch

Hi i am using stm32mp1 has codec which required i2s1 mclk enabled, before codec probe read the basic i2c read chip command need to validate further,note:The board does not have provision to get a crystal to feed MCLK of codec, so thats out of option...

Ara.1 by Senior
  • 1125 Views
  • 1 replies
  • 0 kudos

Flashing (scp) the stm32mp1 from remote server - doing scp from a remote server to stm32mp1 board - uimage,modules,dtbs

Due to office environment and being behind the Proxy I am not able to build and flash (ports locked) STM32MP1 board from my PC at office.I have done the downloading and building of the Developer package at my Home PC (without any firewalls) and wante...

PVaaz.1 by Associate III
  • 2163 Views
  • 5 replies
  • 0 kudos

Resolved! stm32mp157 USB printer support

Hello,​I need use STM32MP157 connect a USB printer. I followed this article(https://community.st.com/s/question/0D53W00000cSjHuSAK/stm32mp157dk2-printer-support?t=1630032775565), and the result is right. but when I use print command like (lp printer_...

xkun.1 by Associate II
  • 2639 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP1 U-Boot freezes while "Starting Kernel" (stalls on "Waiting for root device" in earlyprink)

I have an STM32MP157D-DK1 board, and I'm trying to build a custom Linux image for it with the Yocto Project. I followed the guide here (https://forum.digikey.com/t/yocto-getting-started-with-the-stm32mp157/14074) to create a core-image-minimal.I’m tr...