User Activity

Hello community,I am designing the STM32WL module for the EU868 (south Africa) region based on the LoRAWAN application. As per the datasheet of stm32WL, the max power used in transmitting is 14 dBm @ 868MHz, so with the reference from the Lora-allian...
Hello there.   I am using stm32WL55CC with STSAFE-A110 secure element.   But I could not find any resource for the user STSAFE-A110 with LoRaWAN.   I consider that The LoRaWAN keys (NwkSKey, AppSKey, AppKey ) are generated by STSAFE-A110.   Is there ...
Currently, I'm working on a project in which I have to send and receive data from AWS. In reference to your code, I'm trying to implement my project but, I'm getting errors in middleware like mbedtls_ssl_write returned -0x6d & mbedtls_ssl_write retur...
hello thereI am useing stm32L496 with SX1262DVK1DAS lora module.As firmware, I am using the latest firmeware I-CUBE-LRWAN 2.1.0As lorwan server is am useing public lorawan network.I am testing my device with CLASS_A and CLASS_C modes.my Lorawan peram...
Hello ThereI am using stm32L496RG with Sx1262 and I am using SX1262 stack of I-CUBE-LRWAN.When I try to send multiple data frem to my single node. After the first downlink operation, the second downlink is not received and the code generates the "rx ...
Kudos from