STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

We see dull colours on our LCD, using "modetest" on our custom board, while the colours are bright when the same LCD hangs on the DK2. Are there possible causes we could check? Colour space, gamma correction?

We have made a custom board with an STM32MP157CAD MPU, this board is very similar to the DK2. We have adapted an LCD driver to support our LCD screen, over the DSI interface. It works, both on the DK2 with our own LCD screen, and on our custom board ...

OL'He.1 by Associate III
  • 638 Views
  • 0 replies
  • 0 kudos

Does STM32MP1 support double framebuffer ?

Hi Support Team,Please help me to get the answers for below questions.1) Does STM32MP1 support double framebuffer ?2) If it supports then how can we allocate memories for two framebuffer ?3) If not then how can we avoid tearing effects using one fram...

Shree by Associate II
  • 398 Views
  • 0 replies
  • 0 kudos

Eclipse: undefined reference to

Hi!I am trying to compile a project from several files in Eclipse.Function print_hello() defined in another file N222.Resulting error: undefined reference to `print_hello 'What am I doing wrong? regards Alexander

0693W000000VK3bQAG.png
AShva.1 by Associate II
  • 1884 Views
  • 10 replies
  • 0 kudos

Error: Inconsistency detected by ld.so: dl-lookup.c:

I downloaded, installed and configured Eclipse, Version: 2020-03 (4.15.0), UBUNTU 16.04 LTSWrote a simple program:#include <stdio.h>#include <stdlib.h>int main(void){   printf( "Hello world\n" );   return 1;}compiles without errors :)But, when I run ...

AShva.1 by Associate II
  • 1733 Views
  • 8 replies
  • 0 kudos

The usart1 has issue with PZ6 and PZ7

Hi all, I use PZ7 and PZ6 configure for usart1. But it show some error log.[ 1.633566] stm32mp157-pinctrl soc:pin-controller@50002000: invalid function. [ 1.640375] stm32-usart: probe of 5c000000.serial failed with error -22It's right when II t...

SChen.11 by Associate III
  • 1175 Views
  • 8 replies
  • 0 kudos

Build the ubi system

​I need to build a system for nandflash, unfortunately something went wrong, and I don't know how to fix it

0690X00000DYXNrQAP.png
Yli.8 by Associate II
  • 480 Views
  • 2 replies
  • 0 kudos