STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! OpenAMP u-boot startup

After reading most of the topics concerning my question and not finding an answer, which solves our problem, here my describtion:We are currently integrating OpenAMP in our Application. For now, we are using the configuration from the OpenAMP_TTY_ech...

JMein.1 by Associate III
  • 4532 Views
  • 10 replies
  • 1 kudos

Resolved! PWM Kernel Driver API

Hi all,I wish to perform PWM for certain leds connected to STM32MP1 pins.I wish to do it from the user space application. I got it working via sysfs interface , but I am more interested in controlling it via a user space application based on some log...

NPal.2 by Senior
  • 1323 Views
  • 6 replies
  • 0 kudos

Resolved! stm32mp157 HPLIP support

Hello,​I need use STM32MP157 connect a HP USB printer. New I need install HPLIP package. I am currently using NFS.​But when I use this command "apt-get install hplip", I will receive error infomation. As shown below.​Reading package lists... DoneBui...

xkun.1 by Associate II
  • 1324 Views
  • 3 replies
  • 0 kudos

Resolved! poweroff command line issue

Hello ST Teams!We're testing another one stm32MP1 custom board (battery powered), and i've issue with poweroff command line function:Each time i use this function, board is rebooting instead of poweroffing (...)With these info from tfa:INFO:   Reset ...

Eldam by Senior
  • 2695 Views
  • 5 replies
  • 0 kudos

why M4 firmware been stopped by linux side access uart8@40019000 on STM32MP157C need confirmation of stm32-rproc would stop M4 firmware loaded by u-boot need confirmation on stm32-rproc has issue with kernel 5.10.10

After linux bootup on STM32MP157C custom board with kernel build 5.4.31, I load and start M4 with remoteproc successfully, but every time when linux access uart8@40019000, M4 side firmware stopped, the two command i used to test is "echo 123 > /dev/t...

HZhu.12 by Associate II
  • 1465 Views
  • 2 replies
  • 0 kudos

Resolved! Trace disabled on STM32MP157A-DK1?

I am trying to record instruction traces on-chip via ETF on a stm32mp157a-dk1 board, but the data read from FIFO through RRD is always 0. During the debugging process, I found the value of ETM_AUTHSTAT is 0x08, which means non-secure non-invasive deb...

0693W00000Dpe2VQAR.jpg
Yujia.L by Associate
  • 1019 Views
  • 3 replies
  • 0 kudos

Resolved! stm32mp1 unused pins configure as gpio

Hi I have list of unused pins need to configure as a GPIO, and some as a AF's, do we have any driver which shall facilated unused pins by default set pins state., we have in imx6 IOMUX which does that job in kernel., in mp1 i didnt find that.

Ara.1 by Senior
  • 805 Views
  • 1 replies
  • 0 kudos

Linux device drivers for RTL8211F-CG

Hello. I'm working with STM32MP15-DK1. There is the Realtek IC: RTL8211F-CG. Driver for this IC situates in SDK: linux-5.10.10/drivers/net/phy/realtek.cThere are two defines in this file: #define RTL8211F_TX_DELAY BIT(8)#define RTL8211F_RX_DELAY BIT(...

DFomi.1 by Associate II
  • 4038 Views
  • 1 replies
  • 0 kudos