STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Low Power Application Question

Hello everyone!I had an application that was originally designed to run on a STM32WB55 but found it didn't have the resources we needed for it. The STM32MP1 seems like it has the potential to be a good fit for us as we could do the sensor processing ...

JayDev by Senior II
  • 1676 Views
  • 5 replies
  • 0 kudos

Resolved! USB Composite not working in STM32MP151C.

I tried to probe g_multi to make sure that USB Composite was available.modprobe g_multi file=/dev/mmcblk0The log of the probe is as follows[ 501.458553] using random self ethernet address [ 501.461560] using random host ethernet address [ 501.4806...

rmaki.1 by Associate II
  • 835 Views
  • 1 replies
  • 1 kudos

[STM32MP1] Device tree configuration for I2S peripheral.

Hello everyone,I am currently working with phyCORE-STM32MP1 which has a STM32MP157C mounted.It runs with OpenSTLinux, but it is a modified distribution by Phytec.I have very little experience with handling Device Tree and drivers and my problem is th...

0693W000007ZnW9QAK.png 0693W000007ZnWEQA0.png 0693W000007ZnWTQA0.png
JTánt.1 by Associate II
  • 793 Views
  • 2 replies
  • 0 kudos

How to setup new M4 project on STM32MP157c-DK2?

I have found many tutorials for how to import the example projects into stmcubeide but have not seen much information on how to set up a new M4 project? I have been able to import the OpenAMP_TTY_echo example into stm32cubeide and debug fine but I am...

0693W000007Zi4ZQAS.png
BSunw.1 by Associate III
  • 632 Views
  • 1 replies
  • 0 kudos

How to control GPIO using DT in Application?

I want to control defined GPIO in DT in Applicatoin code. But I can't control this, please let me know how to control gpio with DT in applicatoin. ​1) I can control GPIO in Application without DT . (unused at gpioinfo)2) I can't control GPIO in ap...

BKwak.1 by Associate
  • 589 Views
  • 2 replies
  • 0 kudos

SDIO card not found on boot

Hi,we have a custom board based on the stm32mp151c. It has on sdmmc3 a Silicon Labs WF200 Wifi Card attached. We tested this setup with the stm32mp157c-dk2 and it worked fine. Now, we do not see the message during bootup:mmc0: new high speed MMC card...

0693W000008xHn7QAE.jpg 0693W000008xHqdQAE.jpg
MScho.6 by Associate II
  • 609 Views
  • 0 replies
  • 0 kudos

DAC stops working on M4 side shortly after Linux boots.

This is might save someone the few hours I spent tracking this down. I am wondering if this is a bug. It would seem like a reason that you have m4 sections in the device tree. So linux can be aware not to touch an M4 resource. Linux shuts off the vdd...

BillR by Associate III
  • 691 Views
  • 2 replies
  • 1 kudos