STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Hello, i'd like to use u-boot command sspi to send commands to a spi device with a custom protocol (not a memory). However I see that the command tries to read an ID as it is talking to a flash nor : unrecognized JEDEC id bytes: 00, 00, 00.

Looking at the code, i see file sf_probe.c with .id      = UCLASS_SPI_FLASH, that performs the id reading. How can i use stm32_spi.c with .id         = UCLASS_SPI, driver instead? and send "raw" spi data?

Lmoio.1 by Senior
  • 5254 Views
  • 8 replies
  • 0 kudos

Resolved! Hello, I've exported our custom root filesystem from a running board with the following command: dd if=/dev/mmcblk1p4 of=/usr/local/rtfs.ext4 bs=1M conv=fdatasync

I noticed that after I flash the ST starter package root filesystem, at first boot there is a check on bad blocks and a resize of the partitions, while when I flash the exported root filesystem, there is no checks and some partitions are not resized ...

Lmoio.1 by Senior
  • 1885 Views
  • 5 replies
  • 0 kudos

Resolved! Pin Delay/ Pin Length from die to ball for STM32MP157CAC3 MPU.

Hi,I am designing a product which requires RGB interface length matching. For that I want Pin Delay/ Pin Length from die to ball for STM32MP157CAC3 MPU.If possible please provide Pin Delay/ Pin Length from die to ball for all available pins in STM32M...

DKUMA.11 by Associate III
  • 1452 Views
  • 3 replies
  • 0 kudos

I'm not using USB nor ADC/DAC on the STM32MP157A. Can I tie VDDA, OTG_VBUS, AND VDD3V3_USBxS to circuit ground (VSS)?

If I'm interpreting Table 13 correctly (datasheet p 128), VDDA can be set to 0 volts provided VREF is not used. Similarly power pins related to USB can also be set to 0 volts. Looking in the datasheet p29,I just need to star-connect VDD_ANA, VDD_PLL...

JCond.1 by Associate II
  • 1579 Views
  • 3 replies
  • 0 kudos