STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP257F-DK Power and ST link

Hi all.I am confused about how I am supposed to provide power to the STM32MP257F-DK as it seems I am not providing enough power to the board when connecting the board to my PC via the STLINK/Power connector as the red Power LED is on and the Green LE...

mfny by Associate III
  • 381 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to program the eMMC using STM32CubeProgramer with a signed & encrypted arm trusted firmware and FIP

Hardware setup:- STM32MP257F-DK- The OTP in the chip is burned with the correct OTP value and it is closed.- Connect CN15 USB Port to a Ubuntu Laptop.- BOOT0 = BOOT1 = BOOT2 = BOOT3 = 0- Power on the DEV KIT.Software:Enable Secure Boot + EncryptedROO...

Use LVDS as normal GPIO?

Hi,according to CubeMX the LVDS-pins of the STM32MP25 are not multiplexed, means there is no alternative function available for them.As for my application all this (multimedia) stuff is not needed: is there a possibility to use one of these pins as g...

HMüll.4 by Associate III
  • 157 Views
  • 0 replies
  • 0 kudos