STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems with CubeMX and TIM1+DMA for PWM on STM32MP157 - DK1

I'm trying to get PWM running on an STM32MP157-DK1.When i run the example code "TIM_DMABurst" there is a PWM (had oscilloscope on Pin). Then I configured TIM1 on Channel 1 and the DMA on Stream2 with CubeMX. The generated code looks exactly the same ...

KDehm by Associate III
  • 807 Views
  • 3 replies
  • 0 kudos

Resolved! Some interfaecs becoming disabled while linux boot

I have custom board based on STM32MP153C.This board has 7 serial ports. I configuring these ports with STM32MP1Cube.After linux boot 4 of these serial ports become disabled Driver doesn't probe them and they are in "disabled" state in /sys/firmware/d...

axel101 by Associate III
  • 915 Views
  • 1 replies
  • 0 kudos

STM32MP1 EMMC booting issue in U-boot.

we are working on STM32MP1 in UBOOT 2018 version .we are trying to access the EMMC from UBOOT by using following commands in the below linkhttps://develop.phytec.com/phycore-imx7/linux/pd18.1.0/how-to-guides/flashing-and-booting-from-emmcEMMC is de...

STM32MP1 program few GB image take too long

Hi,For SD, we just take the card to PC, write image directly, take about few minutes for 4GBFor EMMC, we have to use STM32CubeProgram and this take so long, up to an hourI am using USB, not serial. For Serial, it could be a day for 115200bps.We are n...

Dat Tran by Senior II
  • 1064 Views
  • 2 replies
  • 0 kudos

Gcnano driver for openstlinux-5.10.10

We have a custom board developed on stm32mp157 with openstlinux-5.10.10 (dunfell). I want to monitor the GPU consumption, and as per this link, I enabled the debugfs flag from menuconfig. However, upon deploying the image to target, no /gc folder was...

0693W00000WJz6GQAT.png
DKapu.2 by Associate
  • 990 Views
  • 1 replies
  • 0 kudos

DFU mode on STM32MP157F-DK2 - doesn't works

.. previously I had STM32MP157D-DK1 on work, there DFU works Ok,but now bought STM32MP157F-DK2 for home, there's no any sign of connection,reset button do not affect on STlink led, meanwhile stlink/2 itself - works and other USBs - is Ok.Maybe it's a...

valio by Associate II
  • 577 Views
  • 0 replies
  • 1 kudos

FDCAN in production mode is not working

Hi!I am using a STM32MP157C-DK2 board to communicate via CAN. To do this, I have created a program in STM32CubeIDE and set the FDCAN parameters:Classic mode.150KB/s nominal baud rate.HSE clock source (24MH) I have been testing in engineering mode and...

0693W00000WLXyJQAX.png
TArre.1 by Associate III
  • 1443 Views
  • 4 replies
  • 0 kudos

After exec "build_kernel -i" android kernel cant boot

hi ST expert:​I am porting openSTDroid to my mp157 board,i use prebuilt kernel img&dtb and android kernel can boot normal,but when i update the kernel, it cant boot normal,can you help me solve this problem?​my compile cmd:build_kernel mrproperbuild_...

0693W00000Y6pvVQAR.png
ttao.1 by Associate II
  • 643 Views
  • 1 replies
  • 0 kudos