STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PMIC-related issues

The STM32MP135 is powered by PMIC1A. After initial power-up, the voltage at BUCK4 is normal at 3.3V, but during U-Boot flashing, the output voltage at VOUT4 drops to only 2.4V, causing the flashing to fail. The VDD and VDDQ pins of the eMMC are power...

LH1 by Associate II
  • 196 Views
  • 1 replies
  • 0 kudos

MIPI DSI IBIS MODEL for STM32MP255

Hi, I tried exporting the IBIS model from ST website. On importing model to SI tool I can see that there is no model assigned to DSI lines. It is showing NC. Can you share the IBIS model with MIPI drivers in it. or share some IBIS model which I can u...

DJ_IND_0-1758102381709.png
DJ_IND by Associate III
  • 842 Views
  • 1 replies
  • 0 kudos

STM32MP15 SWD Issues

Hi,I recently just finished the Yocto Bringup of a custom STM32MP15FAA1. Everything seems to be working in my application. I am now looking to begin development of the M4 in which I need access to either SWD or JTAG to do lower-level development. Unf...

STM32MP153 DRAM Hardware Question

Hi,I'm designing a board with STM32MP153FAD and have a question about DDR layout reference.Which reference should I follow for the DRAM section?Eval kit MB1272C_03 layoutST's published reference DDR layout.Questions:Which is the recommended reference...

foc by Associate II
  • 267 Views
  • 2 replies
  • 0 kudos