cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP153 DRAM Hardware Question

foc
Associate II

Hi,

I'm designing a board with STM32MP153FAD and have a question about DDR layout reference.

Which reference should I follow for the DRAM section?

  • Eval kit MB1272C_03 layout
  • ST's published reference DDR layout.

Questions:

  • Which is the recommended reference for custom board design?
  • Is there a design guide specifically for STM32MP153 DDR layout and routing guidelines?
  • Is there a document listing pin delays for the FAD series SoCs? This would be helpful for length matching calculations.

Best regards,

Batuhan

2 REPLIES 2
PatrickF
ST Employee

Hi @foc 

please have a look to :

AN5122 STM32MP1 Series DDR memory routing guidelines

STM32MP15x Series DDR memory routing guidelines examples

DDR signals length checker for each packages are provided into the zip file together with routing examples.


You could also check AN5031 Getting started with STM32MP151, STM32MP153 and STM32MP157 line hardware development

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
foc
Associate II

Hi Patrick,

Thanks a lot. I'll check.

 

Regards