STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CCM in stm32mp157

Hi all,If I dedicate the MCU SRAM2 for data and MCU SRAM4 for DMA as shown here, do I get CCM like performance or do I have a risk to have contention on the SRAM2 ?After looking at the bus matrix, I suspect there is no risk but I want to make sure it...

AMART.1 by Associate
  • 1831 Views
  • 2 replies
  • 0 kudos

STPMIC1 - POWER_ON ALTERNATE & MAIN mode

Hi There,When the STPMIC1 goes into POWER_ON ALTERNATE mode via the PWRCTRL pin, does the activation of other Turn-ON condition sources like PONKEY or WAKEUP pins will have a resulting effect to the state of POWER_ON mode? (i.e. also triggers the PMI...

SYEH by Associate II
  • 3111 Views
  • 6 replies
  • 0 kudos

I am tring to rebuild kenel for STM32MP157C-DK2 PC $> make ARCH=arm multi_v7_defconfig fragment*.config

[   1.825627] usbhid: USB HID core driver[   1.833630] stm32-ddr-pmu: probed (ID=0x00140061 VER=0x00000010), DDR@533MHz[   1.840775] optee: probing for conduit method from DT.[   1.844463] optee: api uid mismatch[   1.848396] NET: Registered protocol...

建胡.1 by Associate
  • 1354 Views
  • 1 replies
  • 0 kudos

Multiple camera interfacing

Hi all,I understand that it is possible to interface a CSI2 camera sensor with the camera interface of STM32MP1 using STMIPID02 chipset. Even-though this later support 2 cameras, I'd like to know that it is feasible from the MPU's point of view ?Than...

KLe T.1 by Associate
  • 2562 Views
  • 2 replies
  • 0 kudos

Resolved! after rebuild kernel then machine stop to Waiting for here root device /dev/mmcblk0p6...

I am tring to rebuild kenel for STM32MP157C-DK2 using below url. ​https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Modify,_rebuild_and_reload_the_Linux%C2%AE_kernelAfter I did 5.4 ...

bkwak by Associate II
  • 8877 Views
  • 15 replies
  • 0 kudos