STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The usart1 has issue with PZ6 and PZ7

Hi all, I use PZ7 and PZ6 configure for usart1. But it show some error log.[ 1.633566] stm32mp157-pinctrl soc:pin-controller@50002000: invalid function. [ 1.640375] stm32-usart: probe of 5c000000.serial failed with error -22It's right when II t...

SChen.11 by Associate III
  • 3689 Views
  • 8 replies
  • 0 kudos

How to solve target detection problem?

I have a STM32MP157A-DK1 board. I can't connect to it via ST-Link Utility. It says the target is not detected. Although if I select "Firmware Update" from ST-LINK menu, it updates the firmware of the board (the red-green led blinks etc). But can't co...

0690X00000DYSMoQAP.png 0690X00000DYSNSQA5.png
obingol by Associate
  • 2153 Views
  • 2 replies
  • 0 kudos

Resolved! Debugging Cortex M4 in engineering mode, is it necessary to edit and build device trees for custom modifications?

Hello,I'm trying to connect stm32mp157c-dk2 board with another device over FDCAN in engineering mode (MCU single core) using CN2 pin 3 and 5 (stm32 PA12 and PA11 pins respectively). Though I can initialize and request to use FDCAN1 from resource mana...

MNoor.1 by Associate II
  • 1507 Views
  • 1 replies
  • 0 kudos