User Activity

Hello,I'd like to test your X-LINUX-AI-CV OpenSTLinux image on my STM32MP157C-DK2 Discovery kit as explained in the following pagehttps://wiki.st.com/stm32mpu/wiki/X-LINUX-AI-CV_OpenSTLinux_expansion_packageDo you provide a ready to flash and use X-L...
I need to customize the TF-A en.SOURCES-tf-a-stm32mp1-openstlinux-4.19-thud-mp1-19-10-09.tar.xzOur custom board have a different pin selection for UART4 debug as you can see below, the UART4_TX pin is not on the STM32_PINMUX('G', 11, AF6), but is on ...
I am using the STM32MP157C-DK2For testing purpose I need to build and replace the BSP and in particular the bootloader.The documentation is a bit messy and I'm not able to find the information I need.I need to rebuild and replace TF-A and u-boot.I re...
Koan is proud to provide the unofficial Yocto Project BSP for STM32MP1 based boards.This project is not endorsed nor supported by ST.ST OpenSTLinux is based on OE, our BSP extends the use of ST meta layers with Yocto, using latest commits on the bran...