2020-01-27 7:42 PM
Have been spending time reading the Wiki about the Yocto environment, is there a link to forward technical suggestions and grammar corrections?
2020-02-05 1:02 AM
Hi @KevinA
This Q&A section is the right place to do so.
Thanks to share your suggestions/corrections in a dedicated post.
BR,
Olivier
2020-02-07 10:30 PM
Finally received the new computer, while setting up I found the 'Get Started' needs a link to Development zone/PC prerequisites
After installing everything from Development zone/PC prerequisites I started the Getting started where the first issue was the java 8 install, Development zone/PC prerequisites installed java 11 (sudo apt install default-jre). Next came the STMCubeProgrammer v2.2.0 which is now 2.3.0 and when you run the setup it installs in $HOME/STMicroelectronics/STM32Cube/STM32CubeProgrammer and nothing in the WiKi matches what v2.3 just did...
I added export PATH=$HOME/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin:$PATH to my .bashrc and tested the programmer, ok. The next 'step' was copying the rules so I copied the *.rules since they don't need Readme.txt and version.txt in the /etc/udev/rules.d directory. I think I picked up on everything, I did not install Android, that comes after I get the distribution setup so we can see if our application will run.
Will continue tomorrow - FYI it appears Development zone/PC prerequisites installed everything yet 4.2 USB serial link has me installing again.
2020-02-08 3:55 PM
I started back up this morning but had to stop:
403
Forbidden
Here are some suggestions:
From the Getting Started:
3 Download the SDK
3.1 For ecosystem release v1.1.0
Link: (20 directories below the root of the website, it may have broke from all the pressure at that depth)
I gave it a while and just tried again, nope, still broke.
You really should have a site crawler going to prevent this from causing customer grief
2020-02-08 8:57 PM
403
Forbidden
Here are some suggestions:
From the Getting Started:
3 Download the SDK
3.1 For ecosystem release v1.1.0
Link: (20 directories below the root of the website, it may have broke from all the pressure at that depth)
2 Download the the Linux® kernel source code
2.1 For ecosystem release v1.1.0
403
Forbidden
Here are some suggestions:
I'll move/copy these to a post in the main MP1 forum, nothing is happening here
Basically, if we can't download the files we are just wasting time.
2020-02-09 11:00 PM
Sunday morning the problem was still there and I did some global traceroutes, then IP Whois to discover two groups claiming the IP address, Amazon and cscglobal.com. I sent an email to cscglobal.com letting them know about the issue and by noon it appears to have been resolved. I downloaded the current Source and installed it completing the WiKi to they part of installing the IDE BUT the Wiki doesn't have STM32CubeIDE, Why? I downloaded from st.com and installed but how do I hook into STM32MPU?
The Wiki needs an update starting with the STM32Programmer, no GUI to the install, the SDK has been updated and the source has changed.