STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STLINK-V3MODS for STM32MP1 Compatibility

Hello,I am in process of designing my own STM32MP1 powered device. I was wondering if I can use STLINK-V3MODS as a drop in replacement for ST-LINK/V2-1 in STM32MP157-EVAL reference design. I need the Virtual COM interface embedded in device.-Mark

mhd0425 by Associate II
  • 2483 Views
  • 2 replies
  • 1 kudos

QEMU on stm32mp157

I want to emulate the stm32mp157 on qemu. I have been taking the kernel image and initrd from yocto build, but it is not loading the kernel. using the following commandqemu-system-arm \-M virt -smp 8,sockets=1,cores=4,threads=2 -m 4G \-cpu cortex-a7 ...

Resolved! STM32MP157FAD1

Hello,I would like to ask you few questions since I have some unclearances about STM32MP157F MPU:1. If 933MHz DDR3L RAM was connected to the MPU according to the schematic, will the MPU automatically underclock it to max 533MHz?2. Is it possible to c...

filip1785 by Associate II
  • 2569 Views
  • 1 replies
  • 1 kudos

RPMSG SDB driver failure on M4 restart

Recently I got a problem with RPMSG driver when M5 coprocessor restarts. Thanks to https://community.st.com/s/question/0D53W00000936uRSAQ/kernel-panic-with-pollselect-syscalls-on-virtual-uart-devices-to-m4-core-when-m4-watchdog-restarts?t=16321442601...

mishuk by Associate III
  • 3989 Views
  • 2 replies
  • 1 kudos

DMA Buffer Index with Multi-Channel ADC

Hello!I am using the CortexM4 coprocesor on the STM32MP157F-DK2 to measure multiple ADC channels and update a control loop based on the values. I have set up ADC1 using the DMA2 in circular mode to read channels IN1, IN2, and IN4. I have a buffer set...

jutoroa by Associate III
  • 2851 Views
  • 2 replies
  • 0 kudos