STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Kernel stops loading in middle of boot-up

Hi there,I have a custom board (with eMMC) that freezes in the middle of kernel loading:I am under the impression it is related with the rootfs.ext4, becuase it does not try the loading, but I am not sure yet.Flash table is the following (I don´t use...

Flyback_0-1698682455025.png Flyback_1-1698682634773.png
Flyback by Associate II
  • 1988 Views
  • 1 replies
  • 0 kudos

Resolved! how to access external devices in STM32MP157

hi expertsfor me   this is the first time  to use  STM32MP1 family before i used powerpc-family CPU.with powerpc   when i  attached  external  ICs,   in 8 bit    CPU-A0 to external IC- A0in 16bit   CPU-A1 to external IC-A0 with byte enable signalsis ...

ROAD by Associate II
  • 3962 Views
  • 3 replies
  • 0 kudos

STM32MP157F-DK2 TF-A2 mbedtls > 2.28.2

I wanted to file this on your github page but the issues tab is not available.When using your latest version of TF-A (https://github.com/STMicroelectronics/arm-trusted-firmware/releases/tag/v2.8-stm32mp-r1.1)  self-signing (TRUSTED_BOARD_BOOT=1 ROT_K...

gulsrb by Associate
  • 1727 Views
  • 0 replies
  • 0 kudos

Resolved! stm32mp135-dk board password for putty

i am using stm32mp135-dk board i am install the  STM32MP1-Ecosystem-v5.0.0 Starter Package    now i want to connect the board with my laptop using putty software ,i have the ip address of the board but did't have the password of the board. what will ...

Pooja321_0-1698315844451.png
Pooja321 by Associate II
  • 3381 Views
  • 3 replies
  • 0 kudos

Resolved! GPIO port documentation query: P-MOS is shown inverted but is active high, and vice versa for N-MOS

With reference to RM0436, the STM32MP157 Reference Manual, revision 6.On pages 1066 and 1072 the schematic structures of a GPIO port are drawn (figures 119, 120, and 122). These all show an inverter circle on the gate of P-MOS output transistor and n...

tarmasr by Associate III
  • 5114 Views
  • 2 replies
  • 0 kudos

What is the highest version of opencv compatible with the gstreamer library included in this SDK?

I have transplanted the latest opencv-4.8.1 on the STM32MP135F-DK Discovery Board and run a program to capture video stream from a camera on the borad.I found if I cmake the opencv-4.8.1 source code with "-DWITH_GSTREAMER=ON -DBUILD_GSTREAMER=ON",and...

babai50 by Associate
  • 3074 Views
  • 1 replies
  • 0 kudos