STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32mp157dk2 Ethernet irq poll

Hi!I have been reviewing the kernel log for the DK2 Kit, and I have noticed that the Ethernet configuration is in polling mode. [ 37.074899] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [RTL8211F Gigabit Ethernet] (irq=POLL) Is ther...

AVazquez by Associate III
  • 2212 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP157 DK2 M4 debug issue

Dears,I'm using STM32MP157C-DK2 board in production mode.Now I'm debugging the firmware in M4 core. However, when I insert a breakpoint at DMA interrupt handler and wait for a while, it will crash the whole system (A7+M4) and lead to the reset.I also...

What does "RCC_HSE_BYPASS_DIG" mean?

Hi, I see STM32MP1 - M4 use "RCC_HSE_BYPASS_DIG", what does this mean? And from stm32mpcube, does anyone know the calculation below to get 209MHz?  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;RCC_OscInitStruct.PLL.PLLSource = RCC_PLL12SOURCE_HSE;RCC_...

Dat Tran by Senior II
  • 1560 Views
  • 1 replies
  • 0 kudos

Resolved! Graph is ploting slow in STM32MP1.

Processor Name: STM32MP157 Arm®-based dual Cortex®-A7 32 bits + Cortex®-M4 32 bits MPU Kernal Version: 5.10.10linux destro : openst linuxCrankstorybaord Version : 7.1OpenGLL Version : 2.0Screen Size : 1024 X 768I am developing medical GUI application...

NPal.2 by Senior
  • 2389 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP15 USB driver not loading

I'm attempting to upgrade from ecosystem v2 to v4 and I've run into an issue where the USB OTG port no longer enumerates at boot time. Specifically, I no longer see any messages in dmesg regarding the dwc device, nor do I see anything in /sys/class/u...

MWalk.3 by Associate II
  • 3288 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP157D-dk1 usb to serial adapter

Hi,For the past two days I have been trying to get a usb to serial adapter to work on this board, using both the starter package or buildroot. Whatever I do, it only shows up as new full-speed USB device number XX using ehci-platform. Is there someth...

michelman by Associate II
  • 5116 Views
  • 2 replies
  • 0 kudos