Skip to main content
Associate III
January 26, 2024
Solved

Which is best STM32 MCU for fast driving of GPIO

I need fastest MCU that can drive GPIO pins but not with timers or DMA, just from source. I need to take fast data from a FPGA device. One of determination is max frequency of toggling pin:

I try STM32H562 to toggle pin mode max frequency is around 31 mhz : with this code and core frequency 250mhz:

asm volatile

(

" LDR R0,=0x42020414 ;\n" //GPIOB->ODR

" LDR R1,[R0] ;\n"

"loop: EOR R1,#0x00000001 ;\n"

" STR R1,[R0] ;\n"

" B loop ;\n"

:

:

:"r0","r1","r2","r3","r4","r5","r6","r7","r8","r9","r10"

);

I know too STM32H723 is not the best choise - GPIOs are slower than STM32F427. 

Can some one offer me MCU with fastest GPIOs. and arm core ? Fast as possible.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
January 27, 2024

It's not the instruction speed that's relevant here, its the write buffers, into the bus interface(s) that's going to dictate the achievable throughput.

A GPIO bank attached to the primary AHB is going to be the fastest, unless you have a design bolting them to the TCM.

But again you're approaching the problem incorrectly, you've got an FPGA, make it emulate a high speed bus/protocol that's actually supported by buffering and DMA, and that you can pipeline or FIFO on your side. Be a 32-bit wide FMC bused external memory. Pick a package which permits the widest data bus.

The SDMMC can go 8-bit wide and clock on both edges. Pretty sure it's rated upwards of 100-150 MHz

DSI is running at 250 MHz, two-lanes, DDR, got a bandwidth approaching 1 Gbps

Hard to know where you'd source/sink that much in a continuous mode

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

10 replies

TDK
January 26, 2024

We tried this on a few different chips before, nothing came close to 31 MHz, so possible H5 is the fastest.

Toggling a single pin as fast as possible is not a useful functionality. There are better and faster ways to do this.

"If you feel a post has answered your question, please click ""Accept as Solution""."
mƎALLEm
ST Technical Moderator
January 26, 2024

Hello,

Unfortunately you need at least DMA + TIM for external synchronization to do a such transfer.

Because looking for a simple way by just using GPIOs is not the better method for a fast external data transfers like FPGA or something else ..

You can also use FMC for such data transfers ..

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
January 26, 2024

@Brussl wrote:

 I need to take fast data from a FPGA device. 


So, as @mƎALLEm suggested, why not just have the FPGA put out the data in a more useful/accessible format?

 


max frequency is around 31 mhz :

milli hertz - that's not very fast at all!

:thinking_face:

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
January 26, 2024

This methodology generally isn't desirable as it saturates the CPU with useless work. Sort of thing you do with GATES. 

Writing two different register patterns to BSRR is preferable.

So

STR R1,[R0] 

STR R2,[R0] 

STR R1,[R0] 

STR R2,[R0] 

...

The H7 is one of the slowest, the GPIO is off the M4 Core, so a couple of bus transactions from the M7

The F1/F2/F4 were pretty fast as I recall, but I'd drive patterns via a DMA transaction

The FMC would be a way to do 10's of MHz. Parallel ingress perhaps DCMI

The OCTO / QUAD SPI can be used / disabused in some situations

Some of the newer STM32 have a parallel port PSSI

Perhaps make your FPGA interface actually work in a manner compatible with an available interface method rather than hammer the square peg into the triangular hole?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
BrusslAuthor
Associate III
January 27, 2024

Tnx a lot of all people. As i see F7 is best choice.

With H5 (m33) core I have some "dark" problems. I don.t know why in code above, frequency is 31 mhz when core is 250mhz. First i can't find for M33 instructions duration (clocks). If i use one-clock -- one-instruction then loop  repeat on every 4 instruction , so outpin freq. must be 250/4 = 62.5mhz , or if 'B' instruction is 2 clocks then must be 250/5 = 50mhz.  So i will return to F7 MCU. 

Thank you.

 

AScha.3
Super User
January 27, 2024

So extra for you:   :)

simple hi-lo-hi-lo loop , 250MHz core, optim -O2 , (all setting in IDE "normal", just at max speed) :

 /* USER CODE BEGIN WHILE */
 while (1)
 {


	 GPIOG->BSRR = GPIO_PIN_4<<16;
	 GPIOG->BSRR = GPIO_PIN_4;
	 GPIOG->BSRR = GPIO_PIN_4<<16;
	 GPIOG->BSRR = GPIO_PIN_4;
	 GPIOG->BSRR = GPIO_PIN_4<<16;
	 GPIOG->BSRR = GPIO_PIN_4;


 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }

you see : 4ns pin access, 16ns with while-loop : (bad picture, with a cheap 60MHz-probe)

AScha3_0-1706377849537.png

82MHz - not bad , i would say...

If you feel a post has answered your question, please click on " Best Answer ".