cancel
Showing results for 
Search instead for 
Did you mean: 

B-G431B-ESC1 6-step algorithm

sambit_das
Associate II

I have an A2212 13T motor with B-G431B-ESC1 with  6-step trapezoidal algorithm.It is tracking the speed reference input.

But the problem is that it takes time to reach the desired speed.Suppose currently my motor speed is at 5000 rpm, but if I change the speed to 8000 rpm, it takes time to reach that speed.How to overcome that problem?

 

2 REPLIES 2
MotorRunner
Associate III

Hey @sambit_das  

You must change the speed PI parameters and fine tune them to fit best for your application

Regards!

Gael A
ST Employee

Hello sambit_das,

In addition to what MotorRunner said, I would also recommend you to check your speed ramp value and increase it if need be.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.